Schneider Electric releases pioneering study assessing arc flash risk in 800 VDC data centers aligning with world's leading hyperscalers
- Study provides some of the industry’s first data on managing 800 VDC safety risks and safely adopting new power architectures for AI data centers
- Simulations and arc flash risk analyses assessed two representative 800 VDC architectures reflecting common designs informed by industry leaders
- Evaluating risks with ETAP’s advanced software and digital twins accurately model fault scenarios, supporting effective protection strategies at rack and facility levels
Schneider Electric, a global energy technology leader, today announced a first-of-its-kind analysis that provides practical guidance on how to assess and manage arc flash risk in 800 VDC power architectures. Based on deployment scenarios informed by hyperscaler design patterns, the analysis compares two emerging 800 VDC architectures with varying configurations. Findings demonstrate that arc flash outcomes depend strongly on architecture, capacitor placement, and fault-clearing behavior.
A key result of the research is that even under the most demanding capacitor-dominated assumptions, arc flash risk in 800 VDC systems can be managed, and in many cases, is comparable to typical AC systems. Additionally, better modeling using advanced software and digital twins can help accurately portray arc flash risk.
The findings come at a critical time when 800 VDC architectures are being adopted to support denser racks in AI data centers. Led by NVIDIA, together with energy technology partners such as Schneider Electric, the transition to 800 VDC data center power infrastructure will enable large-scale data centers and AI Factories to support 400 kW IT racks and beyond.
As the industry accelerates toward these higher power densities, 800 VDC distribution has emerged as the practical path to power megawatt-scale racks efficiently. At the same time, higher operating voltages require a deeper understanding of fault behavior, protection coordination, and safe work practices.
"800 VDC power distribution represents a significant shift in data center design, but it also introduces safety considerations that need to be studied extensively" said Manish Kumar, EVP Secure Power & Data Centers, Schneider Electric. "Our work with some of the world’s leading hyperscalers provides engineers and safety professionals with one of the first practical frameworks for evaluating arc flash risks, providing a structured approach to understanding fault behavior, establishing safe work practices, and designing effective protection schemes. Our goal is to help the industry move toward higher-voltage architectures with confidence and safety."
Arc flash analysis is already a standard practice in AC data centers, but no industry-wide standard or guidance currently exists to manage electrical hazards that personnel may encounter in converter-fed 800 VDC systems, making this latest research important to evaluating and managing arc flash hazards, but also ensuring 800 VDC systems achieve comparable safety levels to existing power systems. Current standards are shown to overestimate arc flash risk, whereas Schneider Electric’s simulation analysis demonstrates that advanced software and digital twins more accurately model risk.
Assessment Performed for Two Distinct 800 VDC Architectures
Schneider Electric’s work establishes the first practical arc flash analysis of rack‑level and facility‑level 800 VDC architectures, reflecting the major implementation paths emerging across the industry. The analysis evaluates standards‑based methods, transient simulation, and system‑level modeling. The findings demonstrate that existing arc flash frameworks can be applied to 800 VDC systems when used in an architecture-aware, time-dependent way, and that design choices impact outcomes:
- Rack‑level 800 VDC architectures: In a sidecar (also called power rack) case study using conservative methods and assumptions, results showed incident energy well below the referenced 1.2 cal/cm² PPE threshold, even without protection devices.
- Centralized 800 VDC architectures: The facility‑level case study shows potential for slightly higher incident energy than rack‑level designs when, again, considering a conservative, less realistic architecture with no overcurrent protection. The analysis also assesses the effect of system topology and demonstrates how fault locations both upstream and downstream of reverse-blocking diodes influence back-feed, peak current, and arc flash outcomes. When fault contribution is time-limited with standard protection devices, arc flash energy is reduced to appropriate levels for the work environments and generally aligned with common AC architectures.
Design and protection strategies are important factors for reducing arc flash risks in 800 VDC architectures. The study shows that overall risks remain low, and in many cases are comparable to typical AC distribution. Even with time standard protection devices, incident energy can remain below key thresholds. The research also established that:
- Transient behavior matters: In 800 VDC systems, arc flash is driven by time‑dependent fault currents, with capacitor discharge dominating the first milliseconds of an event.
- Simulation improves accuracy: Software (such as transient simulation and power system analysis tools) shows that simplified arc flash analysis methods for DC systems often overestimate arc flash risk in capacitor-dominated systems. Operators can significantly reduce arc flash risk by informing their protection strategy with advanced software and digital twins like ETAP.
- Design choices reduce risk: Arc flash outcomes depend on architecture and system configuration, not on DC distribution alone, where capacitor placement, reverse‑blocking devices, and millisecond‑scale protection are key levers for safe 800 VDC deployments.
“Industry standards remain essential for arc flash and electrical safety, but traditional methods can be overly conservative because they do not fully reflect how complex DC systems operate,” said Tanuj Khandelwal, CEO of ETAP. “To understand real risk, engineers must evaluate system topology, fault behavior, protection coordination, converter response, switching logic, and active protection schemes. ETAP enables teams to model and validate 800V DC systems as they perform, helping move from conservative assumptions to more accurate, AI augmented, physics-based safety and operational decisions.”
This work builds on Schneider Electric’s decades-long history of arc flash safety testing and bolsters its commitment to supporting the industry’s transition to 800 VDC power architectures, which are a critical requirement for emerging high-density rack systems being adopted for AI data centers. Schneider Electric has also performed extensive testing on live swap power capabilities in 800 VDC systems to enable safe maintenance.
The findings are now available in a white paper titled, 'DC Arc Flash Analysis: A Practical Study on 800 VDC in Data Centers'.
###
Press contact: mediarelations@se.com
- The industry is aligning around 800 VDC for next generation AI data centers. Addressing arc flash risk is essential for safe deployment
- Schneider Electric Highlights Innovation in 800 VDC Power Systems in support of NVIDIA’s next generation GPUs
- 5 Principles for 800 VDC in AI Data Centers: Rack-level Architectures as the Immediate Enabler
- Necessary Considerations for Designing DC Architectures in Data Centers
- Arc Flash Considerations for Data Center IT Space
Related Spokespeople
Manish KUMAR
EVP, Secure Power & Data CentersManish Kumar leads Schneider Electric’s Secure Power & Data Centers segment globally. Manish Kumar leads Schneider Electric’s global Secure Power & Data Centers business, enabling AI-driven compute and AI Factories at scale. He works with hyperscale, colocation, enterprise, and cloud customers to design, build, and operate resilient, high-density, and sustainable data centers during a period of unprecedented demand. With more than eighteen years at Schneider Electric, Manish brings extensive experience across Power management, Smart Buildings, Solar & Microgrids, Enterprise Software, Strategy, and M&A. He combines commercial, operational, and strategic leadership to scale global businesses at the intersection of energy and digital technology. He champions the innovation and convergence of power management, thermal management, and digital technologies as the critical foundation of modern data centers. As AI workloads push density, performance, and efficiency to new levels, he believes innovation in energy systems will determine how responsibly and sustainably the next generation of digital infrastructure evolves. Manish is focused on three priorities: serving customers and partners with speed and trust, keeping pace with AI-driven growth by advancing next-generation AI and data center architectures, and reinforcing Schneider Electric’s role as a trusted energy technology partner, enabling our customers to drive greater impact. He takes great pride in enabling and supporting his team to innovate and do extraordinary things for our customers, partners, society, and our planet. Earlier in his career, he worked in software engineering and consulting at Infosys. He holds advanced management degrees from Harvard Business School and MBA from HEC Paris, and a Mechanical Engineering degree from Thapar University. He also serves on the Supervisory Board of Planon.Read more
Attached files
Schneider Electric releases pioneering study assessing arc flash risk in 800 VDC data centers aligning with world's leading hyperscalers.pdf
PDF, document03/08/2026View asset
Image - Schneider Electric releases pioneering study assessing arc flash risk in 800 VDC data centers aligning with world's leading hyperscalers.jpg
JPG, photo03/08/2026View asset
Contact press
Schneider Electric Global Media Relations
global.pr@se.com
Adoption of Wiztrust's Blockchain Certification Platform
From October 2nd, 2019, in order to secure its communication, Schneider Electric certifies its contents on Wiztrust. You can check the authenticity on the website Wiztrust.com for Corporate communications.
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.